Hello,
On the eval board for MPM3530, on the input, there is Butterworth filter, but according to BOM not all components are putted on the actual PCB. I assume that, these elements are selected during EMC test, but on the other hand in datasheet, I finded EMI test circuit, and there is only one inductor with two capacitors on the input. Is there any way to predetermine the elements on the converter output? DC/DC designer gives input ripple waveforms, but it doesn’t give any proposition for the input filter?
Regards
J