Hi, I’m designing a multiphase buck converter with MP9928 and I have a question.
What should I do with the FB pin of the slave controller? If I understand correctly, the error amplifier of the master controller is electrically connected to the PWM generator of the slave controller through a common compensation circuit (COMP pin), and the error amplifier of the slave controller is turned off when the synchronization signal is applied. So I can leave the FB pin of the slave controller floating?
Thanks in advance.