We are using the MP9488 almost in the same way as on page 18 of the rev1.0 MP9488 datasheet. When supplied with 24 V up to 96 V it works as expected. But if it’s supplied with voltages above 96 V the resulting output is not stable.
The circuit is as follows and should produce a 12V output voltage from a 24-350V input:
It was tested using no load apart from the 3k resistor R1. If supplied with more than 96 V, the output shows the following behavior (yellow = Vout, green = SW):
As L_out we are using the 1mH inductor SDCH1V6045-102M-R, which has a saturation current of 450 mA. Could this be caused by a saturation current that is too low?