Hi MPS expert,
I’m validating a MP8771 SMPS design with 5V Vin and 1.2V Vout. I’ve looked into the R (R1, R2, Rt) and C (Cf) parameters chosen around MP8771 in its datasheet and EV board, and suppose these parameters are optimized basing on 12V Vin.
What I’m concerning is: as the input voltage going down to 5V, ΔI is also decreased. I don’t know if the R/C parameters for 12V Vin are suitable for 5V Vin and ΔI changes to maintain MP8771 working normally.
My questiona are as below:
(1) Can I just use the R/C paramters in MP8771 datasheet Figure 10 or those in EV8771-Q-00A (except R2) for my 5V Vin design?
(2) Is it necessary to optimize the R/C parameters for 5V Vin to get better transient and stability/jitter performance?
(3) If the answer for (2) is yes, can you please provide a set of R/C parameters for me, or educated me how to calculate them with some guidance?
Thanks in advance.