Hi all,
I’m designing a board with a PD circuit that should work in these 3 cases :
- 48V is present between Ethernet 2 pairs (A)
- 48V is present between unused pairs (B)
- no PSE present, so no PoE. Voltage 9-16V present between unused pairs
I was hoping MP8030 was able to switch to ADP “mode” if no handshake is done even if 16V is present on VDD pin.
The question is : Is MP8030 switch to ADP “mode” if 16V present on VDD that risks to make it wait for a potential handshake that will never happen?
Regards,
Michel