I am following the EVL8030-QJ-01A EVK reference design. In bom “TBSG20-155 “ This part has been used. I could not be able to get this part. so could you able to suggest any alternative part for this transformer or can I get the datasheet of this transformer my output voltage is 12V same 70 watts as per EVK (only output voltage is changed from 5V to 12V)
Apologies for the late reply! Here is the EVL8030-QJ-00B which supports your 12V output and MP8030 Datasheet if you are interested.
For the transformer, EVL8030-QJ-00B uses EFD25. I would recommend looking at this post which inquires about the same transformer you are looking for. Past Forum Post
Thank you for your kind reply actually iam using EVL8030-QJ-01A SSR regulation there the transformer used is TBSG20-155 could you able to kindly suggest for this I have not gone through this part TBSG25-40 is because the size of the part is big and it is used is PSR regulation I need compact in size due to my board form factor, thanks is advance kindly share me the equivalent part number for it please