[MP8030] can't full loading

Hi MPS,

I have some test questions and need help from MPS. I was remove LP3 and the output 12V increases the load (with electronic load). It is found that the output voltage will be 0V when the load increases to >1.7A.

The picture below is my circuit diagram, please help to confirm where must be modified.

Thanks,
Richard Guo

1 Like

Hi Richard,

To understand what could be happening, you can monitor the input, output, switch voltage, and load current on a scope.
Removing LP3, there may be insufficient output caps.

If you need further assistance, please submit a ticket to MPS NOW Remote Support - Support.

Best Regards,
Yu

Hi Richard, I am working on a similar device and looking for more information on suitable transformers. I didn’t get any reply or more details from monolithic power team. Who made the UP5 transformer for you? Could you please share with me the datasheet? Thank you very much, Viktor