MP8009a in SSR mode schematic check/help with debugging

Good day,

I have integrated the MP8009a in an SSR forward topology. The circuit was based entirely on the example typical application from the datasheet. However, I am not able to obtain the 5V output on secondary side.

The circuit I have now, uses about 6mA on a 50V input. Every 320ms, the gate is driven by a 10Vpp pulse train for about 10ms. The resulting output is a rise in voltage to 2.2V which then quickly slopes down to 0 in the same 320ms timeframe.

Any help/advice would be greatly appreciated.

Hi Sander,

Can you share the layout with us? We can help you do a layout review to check whether there are any problems. Thanks!

Best,

Fox

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.