Hello,
I am working with the MP8008.
I have copied the reference design with only a slight modification to the inductor and feedback network with the intent to increase the output voltage.
I am using the 750314782 from wuerth. The converter should run at (aproximately)
(Power, Duty, Ip, Fs) = (24, 0.5339805825242719, 1.8727272727272726, 369905.20542221935)
The problem I am seeing is that the ouput is well regulated but way too low.
I seem to have messed up the calculation of the feedback network.
Can you provide example calculations for just the feedback network?
Best Regards