MP7741 split supplies DC coupled application

I am looking for an amplifer with DC to 10kHz bandwidth and high efficiency that can provide +/-10V swings up to 1A.
Can I use split supplies with the MP7741? Is grounding the positive input in this split supply scenario feasible?
I would connect the ‘AGND’ to the negative supply in this case.

Thank you for your help!

Hello,

I don’t believe this is a typical application for this part. I would not recommend connected AGND to the negative supply as the abs max rating is -0.3 to 0.3V.

If you are looking for a BTL, we have solutions like MP7751.
MP7751 | 5V to 26VDD, 2x 20W, Fixed-Frequency Stereo BTL Class-D Audio Amplifier | MPS (monolithicpower.com)

Best Regards,
Yu