Any possibility of stealing some current from the Vcp to run other circuits?
I need ~50mA on V3P3. So, can I:
- Connect VIN_LDO to VCP?
- Connect VIN_LDO to VCP through a switcher (to reduce the current)?
Something like the MPM3606 low current switcher…
I’m sure the amount of current I can steal is a function of the switching frequency of the PWM into the MP6543…
Other questions:
A. What is the PWM frequency VS power consumption?
B. What is the maximum PWM frequency?
C. What is the drop out voltage and PSRR for the V3P3 regulator?
D. If I cannot steal 50mA, how much can I steal?
I have multiple MP6543’s on the board, so, perhaps I can load share.
Thanks!