Hi i am seeking to develop a flyback converter.
Vin 30-60
Pout is 120W
Vout 12V 10A (max ) 5A Avg
At this stage i was learning towards using a MP6005 for this application in a flyback configuration with primary side regulation.
I would like to adjust the reference design EV6005-K-00A to meet my needs in this instant. Do you think this is possible? I understand the power stage will need to be re designed (transformer, Snubber, mosfet, Rsense)
Are the calculations available for the reference design to work against ?
The comp pin components how are these values determined calculated ?
Thanks