Hi,
I’m using the MP5030 for an application that is only 5V. I have connected everything as per the reference design however I have left the adj pin floating as there is no need to change the input voltage. When the MP5030 is operating normally below 5.5V the device has a small quiescent power draw (uA range) but when I go above the 5.5V it starts to draw over 75mA.
-
Why has the current consumption increased so much? It says in the datasheet that the IN and OUT pins are 16V (absolute maximum)
-
Why is the test pin tied to VBUS when VBUS can be 3-12V for QC 3.0. The datasheet does not say that this pin is 16V tolerant although I have tried to limit with a zener to fix 1.