Dear Sirs,
There are description about sleep mode in MP5016H datasheet page 14 as following ===.
But, I cannot find any description what 'sleep mode ’ is , in the datasheet.
Whichever, I will check using EVKT also.
=====d/s page14 ======
The current limit cannot be set
too low, because the MP5016H works in sleep
mode when the load is lower than 0.38A,
typically. The current limit logic is disabled in
sleep mode, also.
Best Regards