In the datshheet FEATURES of the MP4582 there is shown “1V to 30V Output Voltage Range”.
Is there an application availble for a design with an output voltage of 24 V up to 800 mA ?
Hello,
There isn’t a specific application design for 24V. But, you can change the FB resistors to get 24V output at 0.8A.
So, you can fix R1=230k and R2=10k for getting 24V output.
Let me know if you have anymore questions.
Regards,