Hi there!
Im planing to use the MP4560 on my board.
Here you can see the schematics.
i hope this works…
I think everything will work quite good but the only think i cant calculate are the parts on PIN COMP.
C27 and R16
Requirements:
Can anyone here help me?
Thanks!!
Some rando on the internet. I would double check D9 I would think it should be connected to GND and SW not FB and SW.
I would double check the boost pin, I think there should at least be a cap between the BST pin and the SW pin.
Check the voltage of the input caps, 50V cap on a 48V line will stress the caps, consider double the voltage or triple for reliability
Hello pascal.player,
Please see the section titled “Compensation Components” on page 12. There is also a DC DC Designer Online model that can help with initial selection. You will need to tune it get proper real world results.
Thank you,
Vinh Tran