The MP4559 provides 1.5A output current.
Datasheet Rev 1.01: The Ilim is 1.9A typ (duty cycle <60%). There is no graph of the Ilim.
We have an avarage current of 400mA and peak current of 1.9A for 5 ms duty cycle 12%
In the DCDC Designer Online the “High Current of Transient” is limited by 1.5A, so we cannot simulate/verify this.
Can you confirm if our 1.9A peak current is possible with the MP4559?