I am designing the power supply with 14v output voltage and up to 5A current but there is a problem that output voltage heavily depends on the load current and changes as much as by 1V.
At the higher currents pretty high PWM jitter is observable.
What can be causing this problem?
My PCB is not as compact as suggested in the datasheet to improve thermal performance (inductor is moved slightly further away from the IC because it gets very hot.) and electrolytic capacitors are used for both input and output. which should be better for this chip
External Ramp Compensation uses DC Blocking Capacitor (0.1uf)