MP4317: Synchronizing two MP4317

I have a question about synchronisation of two MP4317 in close proximity (1st converts to 5V, 2nd to 8V). I have connected SYNC OUT to SYNC IN with a 100Ohm resistor, hope this is correct. But what about the MODE (AAM/FCCM). Could I still run the “master” in AAM-Mode? I would assume FCCM mode is most advisable in sync mode. If AAM-Mode is possible, how do I setup the “slave” unit mode?

Hello @h.andreesen,

I believe the implementation of the MP4317 in a multi-phase configuration seems impossible as this part does not support multi-phase. What is the end application, input specs and output current? Based on that, I can recommend another part which might be potential fit for your application.