Hi,
I would like to ask which part variants (MP5031GRE-xxxx, MP4245GVE-xxxx) would be required for up to a 60W USB-C PD output from an 8 - 13V input, following this reference design:
For the required part variants, could you please send the configuration tables for the registers so that I can determine whether this part can be used without programming in my application? Can this reference design be directly copied for a fully working 60W USB-PD source from a 8V - 13V input, or are there any other safety / configuration settings I might need to add?
Thank you so much, have a great day.
Hello haase.industries,
The MP5031 will detect the device that is connected and establish a contract. It would need to determine what is appropriate for the device then it will reconfigure the DC-DC converter (MP4245) to support this. So given this information the device would need to be reconfigured in order to be able to supply 60W. I have still provided the configurations for the different suffixes available.
The MP5031 would require configuring the slave device from the slave_device_sel register shown below. Given that the MP4245 is part of MP424x it should not need to reconfigured as this is the default.
Thank you
1 Like
Hi Eduardo,
Thank you for your reply. I will send the schematic here for review when I finish it, if that’s ok. I will be using the 0000 variant of MP4245 and the 00A3 variant of MP5031.
Have a great day!
Kind regards,
Rain.