MP3438 Vin to Vout gap

Hi all,

I put this topic in “power converter” as it’s the primary use of the MP3438, even though i’ll use it as a led driver using current sensing.

Context : MP3438 powered by a lithium cell (3.5 to 4.2V), to drive a Cree XHP50 LED, 6V (more like 5 to 6V in my current range). Current ranging from 10mA to 1.5A

The mp3438 being a boost converter, that should roughly work.

The datasheet, page 6, bottom-right graph shows the current limit depending on the output voltage, for 2 different input voltages. For the Vin=3.3V curve, Vout starts arround 4V. For the Vin=6.6V curve, Vout starts arround 9V. Why is the gap so big ? Does that mean the mp3438 can’t power a 8V load from a 6.6V output ?

  1. What would happen when the battery is full at 4.2V and i try to power the led with low current, at 5V ? (Note : the MP3431, often used as a led driver can do that)

  2. For other input values, how can i calculate the minimum reachable boosted output before going into (non boosted) pass through mode ?

Thank you for helping !

Hi,

The boost converter will work for your 6.6V input, 8V output.

  1. At a low current, or light load, the boost will work in power saving mode (PSM). This is activated when your inductor current reaches 0A.
  2. Pass-through mode is activated once the input voltage exceeds the set output voltage. Your input voltage will dictate the minimum output voltage.

Best,

Tyler

Hi Tyler,

Thank for this answer. I’ve also red that this gap can be calculated using frequency, inductance value etc apparently.