Good morning!
I have some problems with MP2905 IC:
- It always starts only with open-circuit on the load side. When some load applied at off state it sometimes starting at first time, sometimes not. Then it starts every one time.
- When I raise the output current to about 1 A the IC goes to failed state when there’s only a few impulses on the inductor at about 4 MHz and nothing more (see pic attached). Then I have to decrease load to about 0.2 A and MP2905 starts working. I have schematic made by the second scheme from appnote and it supposed to provide as much as 12A load current. My scheme is calculated for the output current 3 A.
I tried to choose another inductor SRR1208-6R5 from Bourns and the current threshold raised up to about 1,5 A that is too far away from 3 A.
I’ll be very appreciated if you could help me. Thank you!