Hello, we are currently considering MP28167-A for use in a test device that will supply 3~20V voltage to DUTs by directly connecting to DUT rail. The DUT rail may or may not have power already.
I’m wondering whether MP28167-A can handle the following scenarios without damaging itself, become unstable, or causing current backflow to IN:
- MP28167-A unpowered but DUT is powered
- MP28167-A powered and DUT is powered by another source, with very close voltage to MP28167-A output setpoint
- MP28167-A powered and DUT is powered with a higher voltage than MP28167-A setpoint (<23V)
We can insert an ideal diode after OUT, but it will be nice to save one extra IC if the converter can handle this.
I would also like to ask whether it’s the same for MP28167, MP8859, MP8860/2, as these SKUs seem to have the same die.
Thank you!