MP2790 Not able to write registers

I am working on getting our new BMS with the MP2790 up and running. The issue I am having is that I cannot set registers or trigger ADC conversions in the part using i2c. What could be the reason for this?

Here is my procedure:

using the MPS GUI:

On MPS2790 eval write cells 7-1 enabled to register 0. Then read back using GUI and get correct cells 7-1 enabled.

On my BMS board write cell 7-1 enabled to register 0. Then read back using GIU just provides the default value again.

On MPS2790 eval using GUI I can get the ADC to read and get back all cell voltages. On my board the GUI never provides cell voltages and reads back 0V.

Thanks,

Richard

Hello Richard,

Let me look into some possible causes other than perhaps double checking the hardware connections that would cause the ADC readings not to be read.

Will get back to you on this soon.

Hello,

You had mentioned that the EV2790 and the GUI worked fine the first time.

When I mentioned checking the wiring, First, I would start with the battery.

Then double check on the following:

  • VDDIO and VDD are powered and stable.
  • I2C ACKs transactions via a scope or logic analyzer. Verify that you have proper pull-up resistors are in place. Use the EVB as a reference here.
  • Also, double check that the I2C slave address is correct.
  • Be sure the RESET pin is properly deasserted. Some designs leave this pin floating, but please check the evaluation board schematic here for reference.
  • Cell Input Wiring for cells C0 - C7 needs to be properly connected and biased. Otherwise, ADC conversions may fail, resulting in 0 readings.

We can start with these debugging steps and go from here.

Best,

Krishan

Hi Krishnan,

I got it working shortly after posting my question.

Thanks for the assistance though.

Richard

Good to hear Richard,

What was the fix in this case? Just curious is all.

This behaviour can also be seen if you enable CRC and write it verbatim per specsheet. The specsheet on page 39 is wrong. You need to exclude the first two bytes shown in the check sequence.

It was a solder issue I had elsewhere on my board.

I had question regarding the use of the MP2790 in a series / parallel pack configuration. Should I start a new thread for this?
When using the GUI and the EVAL board I get a “FET driver failed fault” error when there is a high capacitive load or voltage present on the Pack output. In parallel pack configuration, voltage may be present on PACK output before enabling the Vpack of the battery.

Thanks,

Richard

No worries there Richard, I suppose even if this isn’t a different subject this is sort of an update pertaining to your project.

The “FET driver failed fault” error that you see is actually expected.

The MP2790 tries enabling the PACK FETs into a pre-charged or capacitive load. If PACK is already at the voltage or Cout is large, the gate driver may not fully turn the FETs on (within a timing window in which it should in typical conditions), resulting in this fault.

You should actually be able to verify this by repeating this with your capacitive load removed.

Increase the TURNON_TIMEOUT or add some pre-charge path to your PACK capacitance before enabling the FETs. Another way to fix this could involve some RC network to slow the slew rate down for the FETs.

Either way, however you can, mitigate the inrush / abnormal VDS conditions that trigger that fault.

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.