Hi MPS-Team,
We’re working with the MP2787 on a new product for a customer, we have a strange issue where in sleep mode we are seeing current of ~17mA through the cell taps.
We are using 200 Ohm RCELL_FLT resistors with 100nF CCELL_FLT capacitors which have both been checked as correct.
Schematic:
The connection that goes off the screen to the top of the image goes to an ORing circuit which is currently out of use and separated.
“Vin” feeds a buck converter.
These shouldn’t impact the current drawn from each cell tap? The only path for current that I see is through each tap into the IC?
Any help is greatly appreciated.
Thanks,
Ben