MP2761 NVDC Controll

Hello

My customer consider to use MP2761.
They have a some questions.

I checked the datasheet, but I don’t quite understand NVDC mode.Could you please explain how this operation works in detail?

Q.1

Does the MP2761 limit the current for the SYS pin?
I understand that the OCP functions include the switch current limit and the input current limit.

Q.2

Does NVDC mode support the system when it is overloaded by pulling power from the battery output?

If so, how much output power can the NVDC architecture support?

For example
Vsys=8V
Isys=6A Max (Reccomend value in the MP2761 datasheet )
So,I understand maximum outputpower is 48W typically.

Can the battery supplement mode support a power level exceeding 48W?

We want to support a peak power of over 80W(Vsys=8V, Isys=10A).

Can we use the MP2761 under this condition?

Thanks.

They are now considering the MP2764 instead of the MP2761, so I’ve updated the information.
Please take a look at the new thread for MP2764.

Best Regards.

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.