Hi,
I have a questions regarding the startup behavior of the MP2760 and need to ensure that the device can perform up to the requirements.
Requirement
System implements multiple behaviors that transition between power states.
In one particular state
- System must be completely powered off
- USB C reconnect is the only wakeup event to exit that state
Strategy
- Disconnect battery by disabling BATFET (forced turn off by setting
BGATE_ CTRLin the configuration registerREG10hto1).
If V IN is absent, the MP2760 is no longer able to generate its VCC and is completely powered off ==> system is dead. - On USB C reconnect, MP2760 can generate VCC from VIN and boots and generates VSYS which then causes the other system components to boot ==> system is alive.
Question
-
When
BATFETwas forced off via I²C, will the MP2760 reset theBGATE_ CTRLflag to0after a reset to reconnect the battery or will it sense a missing battery and fail to restart asBGATE_ CTRLis persisted across resets? (I expect all registers to be set to default after a power cycle reset) -
Regarding the “Missing battery detection” feature: will the MP2670 halt or continue to operate and feed
SYSwith VIN when battery is not present?
From the datasheet:Battery Missing Detection
The MP2760 counts how often charging
terminates every 10s. If charging terminates
more than three times in 10s, the MP2760
reports that the battery is missing in the status
register and initiates an INT signal.Based on my interpretation that means that the MP2760 infinitely loops through 10s cycles trying to detect the battery where within each cycle the battery presence is asserted >3 times. And in addition, after every 10s cycle the INT signal is issued. Then cycling stops once the battery was detected.
However, whether VSYS is populated during the absence of a battery is not clear.
Also whether MP2760 continuous charging after connecting a battery is not clear. There are sources that state that similar MP devices don’t tolerate a battery connect event after startup.
Furthermore, will disabling BATFET (and therefore disconnect the battery) also trigger the “missing battery” detection? I assume the MP2760 senses theBATTpin, which should have a valid VBATT independent from the state ofBATFET?
Will connecting a battery also raise INT?
This is the only uncertainity I have and that I like to sort out before ordering the part for further evaluation.
Thanks for your time!