Hi,
We have designed a 4S2P battery charger using the MP2759A charger IC combined with a TI BQ77915 Monitor IC.
Number of Cells: 4
Cell voltage: 4.2v (16.8V pack voltage)
Charge Current: Set for approx. 2.8A
The charger starts to charge at 2.8A but then the current drops to 20mA {nominal load) and the STAT pin pulses at 8Hz as shown below. Includes schematic.
If I connect the load, which is minimal around 30mA the battery charge is stable util the battery voltage increases to a point where the pulsing starts again and the battery no longer gets a charge current even though the battery is not fully charged.
What could cause the STAT pin to pulse.
Note: If I remove the NTC, the charger IC STAT pin blinks at 2Hz error rate.
Any help would be appreciated.
Thank you
Regards
Carl