Hello,
I would like to charge a LIFEPO4 battery pack 3s with the MP2759. I got the dev board and i made some changes for my application. I don’t need to have the primary path from VIN to VSYS, so i made this change:

I plug the 12V input and i see ACOK and STAT led solid ON (this mean that the battery shall be in charge). I just changed the VLIM jumper to 15V but the others are still the same as the beginning.
Do you have an idea why it is not charging? Do i really need to connect PMID pin to something? I took a like on the internal schematic and this shall be good to keep only the decoupling capacitor.
thanks you.