What should be done to configure the MP2731 to use either 2.1a or 2.4a for nonstandard charging? Is this something that can be done using the registers or does a voltage need to be applied to the DP and DM pins?
Hi mbaker,
Thanks for posting on the MPSNow Forum.
There is a section (Input Source Type Detection) on page 21 of the datasheet that goes into detail about this.
You can force DP/DM detection using the USB_DET_EN bit[5], and then change the input current limit using register VIN_STAT bits[5:7]
Thanks,
Cindy
Thank you for this info.
It turns out for non-standard charging I didn’t have to do anything other than up the current limit to have it deliver more current.
1 Like