MP2731 compatibility with 1.8V microcontroller

I am hoping to confirm if the I2C bus on this DC/DC is compatible with 1.8V levels? I have a low power microcontroller running off a 1.8V supply and I would like to interface without the use of level shifters (for cost efficiency and board space).

Hello adownengineering,

Thank you for visiting the MPS Technical Forum. Please see from Pg. 10 of the datasheet the Electrical Characteristics table below. The SDA/SCL pins can support up to 5V, but it just so happens the pull-up voltage sample condition we use in the table is also 1.8V