I appreciate your support in the past. I am working on bringing up the board which has MP2722 as the charger IC.
MP2722 works with a USB-A charger but I have an issue with charging the battery using a USB-C charger and USB C to C cable.
When I connect the board to a USB A charger using a USB C to A cable, VBUS 5V is on and MP2722 works fine. The input current limit is 2A. When I connect the board to a USB C port on a PC using a USB C to C cable, VBUS 5V is on and MP2722 works fine. The input current limit is 1.5A.
However, when I connect the board to a USB C charger using a USB C to C cable, the voltage on CC pin is 800mV voltage on but there is no VBUS. Could you please advise what I should do to work with a USB-C charger? Please check the sch and let me know if you need any information from me.
Thanks a lot.