Hello, I have been working around with MP2722. It is working perfectly. I need to charge an external device (eg. Smartphone) and it is charging the device with no errors at all. I am charging the smartphone with a 2000mAh battery. So I facing a tiny problem.
Issue is that I am having a LCD Display in my system. When the external device is connected and the battery voltages drop below 3.3V then my display starts to flicker, I don’t need that flickering at all. For that reason. I want my MP2722 to stop the charging once the voltage level reaches at 3.3V.
I have configured the 0 position bit(EN_CHG to 0) of REG09H register unfortunately it doesn’t helped me. As I couldn’t understand the behavior. So I implemented the condition that if voltage levels reaches to 3.3V I have configured the CC_CFG[2:0] to Disabled.
So basically now I want your suggestion that if there is any way around other than the above mentioned from which I can stop the external device charging. Thanks
Best Regards
Muhammad Haris