MP2672AGD does not charge

I’m charging 2 LiIon cells with MP2672 with a typical 5V USB, but the current meter does not show any current.

For a 5V USB I measured:

Column 1 Column 2
PIN Voltage, V
IN pin 1 4.7
SW pin 2 6.0
BST pin 3 4.7
MP_VCC pin 4 3.6
VLIM pin 7 2.3
NTC pin 8 1.8
MID pin 9 4.0
BAT pin 10 7.45
SYS pin 11 7.7
STAT pin 16 1.4
CV pin 17 0.3
ACOK pin 18 0.16

Pins 10 and 11 might be swapped in the table above, need to check.

When I increased the USB voltage to 5.4V, I saw 250mA current in my current meter.

I used the schematics I found somewhere and there VLIM was a simple voltage divider 1k/1k. So did I. Not sure if it’s correct though.

BALLANCE_EN is pulled low and controlled with an external GPIO I2C expander - I couldn’t come up with something smarter to

  1. automatically charge on start when USB power rail is powered

  2. allow the user to configure charge settings if they want to without any jumper (they don’t have access to the hardware)

P.S. I looked at similar topics here but didn’t find the answer.

Hii…did you got solution for this? i am also facing the same issue…

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.