MP2672 - Overshooting / OVP

Hello,

I encounter a problem with the 2s Li-ion charger MP2672. When connecting the VBus, the register 04H bit 3 is high meaning that the ic entered the battery overvoltage protection and stopped charging. When mesuring the voltage battery alone (charge disabled) I get 6.7V.

Here is a dump of all the registers :

REG 0 : [0…7] 0011100

REG 1 : [0…7] 11110001

REG 3 : [0…7] 00000000

REG 4 : [0…7] 00010001

You can see in the attached files my schematic and layout.

Do you have any suggestions on why this behavior happens at random interval (sometimes at power up, but also a few seconds later) ?

Hi,

What are the individual voltages of your HS and LS cells?

Best,

Tyler

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.