MP2672 getting above 100°C while charging

Hello,

I’m working a project, where I would like to use the MP2672 to charge two 18650 cells in series. My problem is that MP2672 gets hot quickly (in 2-3 seconds to above 100°C) even though I’ve set the charge current to 500mA.

Here is the schema:

I’m aware that C14 is at the wrong place, it should be between IN and GND. This is due to an error in the original schema which I had to work around but I would not expect this to be the cause?

V_IN is attached to a 5V USB-C Notebook charger. It should be able to provide enough current. V_BATT and V_SYS are connected to a disabled circuit.
The solder bridge JP3 is closed connecting the 24k resistor to ISET which should give a charge current of 500mA. ACOK and STAT are connected to two LEDs. Both of them are solid on as soon as V_IN is connected.

This is the inductor I’m using: https://jlcpcb.com/partdetail/Sunlord-MWSA0603S1R5MT/C408444

If the batteries are not in place, MP2672 gets to about 30°C. As soon as the batteries are connected, it heats up quickly to above 100°C. The heating also happens If I add a load (< 500mA) to V_SYS without batteries installed.

I’ve already compared my schema with the reference design but could not find the error. The same issue happens on two different PCBs.

Since I’m a hobbyist engineer, I’m a bit lost on how to further debug this. Would be great, If someone could guide me to the right direction.

Here is also the layout of the PCB around the charger:

Probably not optimal but hopefully good enough to not cause such an issue.

One additional remark:

I have left pin 12 (SW) unconnected and only used SW on pin 2. The datasheet seems to do the same in the reference layout:

Is this ok?

Au Contraire, I do expect it to be the cause. That will cause massive switching loss in the FET at least get rid of C14 and see what happens. Plus do you have a EVAL board? These are super useful tools I know they are expensive but how much are you spending now?

Yeah thank you very much. This indeed was the issue :slight_smile: No, I don’t have an eval board. Currently, it looks like my issues with this IC are solved. If not, I might look into one.

You should really look at a common GND. The Chip, The output caps… same piece of copper. Look at the snippet below… Also 3 capacitors → 3 vias minimum and route the skinny track outside the GNDS - straight line connections between input, output and chip

Thanks for your input. I have already adapted my layout to match more the one in the datasheet:

I’m not sure what you mean with skinny track outside the GNDS and the straight line? Is this already solved with the new layout?

1 Like