Hi,
I would like to ask if there are more “steps”, which must be performed before writting 1 to Bit5 on REG 06h, to go to Shipping Mode? (ex: Disable Charge by set 1 to Bit3 on REG 01h)
Many thanks in advance,
Nathan
Hi,
I would like to ask if there are more “steps”, which must be performed before writting 1 to Bit5 on REG 06h, to go to Shipping Mode? (ex: Disable Charge by set 1 to Bit3 on REG 01h)
Many thanks in advance,
Nathan
Hello Nathan,
The MP2667 can be put into ship mode via I2C, there shouldn’t be any additional steps other than what is written.
Please see the “Battery Disconnection Function” in the “OPERATION” section of the MP2667 data sheet. I2C programming can be done using our GUI and the EVKT-MP2667 kit
I hope this was helpful.
Kind regards,
Eliza