Hello,
I’m currently designing a 2S USB-C Power Bank using the MP2651 IC alongside the CCG3PA PD controller. This design, inspired by the MEZS7-1S-4SPDPowerbank, seems like the perfect choice for charging and discharging a power bank utilizing the USB PD 3.0 standard. In my design, I want to support Battery PDO as the source with Fixed PDOs (5V–20V) for both source and sink.
The questions are as follows:
-
In source mode operation, how can I set the output voltage (VIN_SRC) to follow the battery pack voltage (VBATT)?
-
Can I enable Q1 and Q3 to be always on so that current can flow from the battery pack (CFLR) to VBUS (IN)?

-
Or can I set the value of the Output Voltage Setting in the Source Mode register to be the same as the ADC result of the battery voltage?