Hi team,
I tried to use the MP2639A for two-port application (charge and discharge) with two Li-Ion cells.
If charging voltage (5 V) is present at VL, VCC = 4.5 V, if no charging voltage is present (discharging), but only the battery voltage at VH (VH = 7.6 V), VCC = 120 mV. Without MID pin connected, VCC = 0V.
Does anyone know, why VCC is not 4,5 V, if opperated with batterie?