Hi,
I have MP2617H on my circuit to charge 18650 battery up to 3.7V however I am seeing that the CHGOK starts flashing after a period of time.
Here is the circuit
Additional info:
Supply Voltage: 12V
Max Input Current: 2.5A
Max Charge Current: 2A
NTC: 10k
Mode: Default
Output Voltage: ~3.7V
I think some of the resistors may be wrong value, but can’t determine which ones?
Any advise would be much appreciated.
Thank you