I am experiencing an issue with my schematic when supplying power via USB (5V input). The Vout pin is not reaching the expected 4V, even though I have configured the voltage divider (R11 = 25.5kΩ and R16 = 10kΩ). Currently, the SYS pin voltage is 3.6V, but I need it to be 4V.
Could you please review the schematic and suggest any modifications to achieve the desired 4V output? Also, please note that I am supplying power only through USB and have not connected a battery.
What is the SoC and voltage of the battery? Vsys is not completely a regulated voltage output. Vsys stays at 3.6V whenever Vbatt is equal or lower than 3.4V. Then Vsys follows Vbatt afterwards according to this.