Hi, I have a question about my latest circuit. I tried to use the MP2615 to charge 2 18650 batteries with the S-82A2AA-A8T2U primary protection chip to prevent overcharging and overdischarging.
Right now, I have a problem with the connection 2 battery for the first power on time; it can’t charge the battery, and the VBAT-=-4.7V and VM-=-0.6V, the S-82A2AA-A8T2U chip OD mosfet discharging controller is low, which can’t make the VBAT-connect to GND to initialize the work.
I looked at the S-82A2AA chip, and it said, “Caution: After the battery is connected, discharging may not be carried out. In this case, this IC returns to the
normal status by connecting a charger,” but I connected the charger and am still not able to work.
So, can you help me figure out what the error is?