Is there a spice model available for the MP24971? It would be nice to simulate some deviations from the standard circuit.
I want to use a voltage divider to force the device to higher output voltages than the constant 5 V. I would love to have it adjustable between 20 to 30 V instead. Or is there another device available with output voltage adjustment in this range?
I also need the functionality of output current detection / limitation but I want to use the device as a controller for a high-side driver only which controls a MOSFET cascade to generate 200 to 250 A. I want to set a current limit at 250 A. I guess I can use the MP24971 functionality for this with a well designet shunt resistor
Another function I miss is the undervoltage lock-out, which I would like to set to 30 V input voltage.
Thank you in advance
Gunter