Hello. I am using the MP2494 in a very similar schematic to the evaluation board.
I have a problem when the board is powered with more than 12v.
Sometimes the IC will simply fail. Othertimes the pin 3 (EN) will blow up.
The board draw almost 2watts at 22v.
I have connected EN to VIN as per page 7 of the datasheet:
The MP2494 has an Enable control pin (EN). Drive EN above 1.8V to turn on the MP2494. Drive EN below .4V to turn it off. Tie EN to VIN for automatic start up.
But in the absolute “all other pins” are rated as +6.5V…
Now I am confused. What is the rating of the EN pin?
When VIN > 6.5V how can I enable automatic startup?
I’ll have to make new boards now ![]()
Thank you in advance for your support,
Maximilian Schneider