But they let the magic smoke out after 1-2 seconds. Do I have an tremendous fault in my schematics? Or is the MP24833A not suited for this. The PWM dimming is done by a 3.3V MCU
If the MP24833 is not suited, is there another one? Minimal external parts and up to 3A Buck Boost LED driver?
Are the two MP24833-A used for two different systems/LED outputs?
Do both the devices have the same operating conditions? What is the switching frequency of the PWM dimming signal from the MCU?
Yes different LED-String, both identical.
Should be same operating conditions, same supply identical, but independent, LED-Strings.
ATmega 328p with 490Hz.
Hello,
Tried this on the PCB I designed, since the schematic looked so easy, that I didn’t thought about using a proto board. And no didn’t use(bought) the evaluation board because of said reason, in hindsight a mistake.
High Current is relativ, it drew like 20% more current than anticipated 650-800mA. The IC lit the LED string up, sometimes 2-5 seconds and then bruned up. My oscilloscope is currently in repair after it was damaged, so I couldn’t observe the waveforms