I inherited product ownership for a design from an ex-colleague which incorporates a MP2481 LED driver. Input voltage is 12VDC. Connected LED chains consumes approx 260mA at -18.6V.
When I follow the datasheet it states to choose my ripple current to be approx 30% of my max load current. Since my max load current is pretty steady at 260mA that would be 78mA.
The datasheet a states as well how to calculate the inductor and when I follow these formulas I get to an inductance value of 66uH. That is considerable higher than the 10uH the datasheet mentions
"If the calculation of above equations results in an inductance greater than 10uH, a 10uH
inductor is still preferred."
When I, after some browsing, repeat this calculation using the values as used in MPS Publication “AN009, Wide Input Voltage Range White LED Driver Solutions with MP2481” I get the correct results. In this example the load current is 250mA. However, these calculations use a ripple current of 0.6A. That’s such a large ripple that one can even discuss if “ripple” is the correct term to use.
But in the end my issue is that the used inductor (10uH, DCR=400mOhm, Isat=1.4A) is getting quite hot. Replacement with a 4.7uH, (DCR=200mOhm, Isat =1.4A) does not impove things. I definitely could improve things in my physical layout but the inability to determine a correct coil value still gives me the feeling I’m far from being on top of things.
Anyone who can shed a light on how to deal with this ripple current selection?