How can I calculate the values for resistors, capacitors, and inductors in a power supply circuit using the formulas provided in the datasheet, when I have a 24V input supply? Additionally, how would I adjust the calculations if I use a 19V input supply instead? Please explain the steps for each component (resistor, capacitor, inductor) using the datasheet formulas."
Hello,
You will need to follow all formulas in the MP2393 datasheet from pages 12 to 17, which should be explained in full detail which covers all relevant resistors, capacitors, and the inductor.
For all components that are not covered by the formulas that in the following 5 pages I have directed you to, please see the pin functions on page 3.
All typical applications for this part from pages 18 to 20 operate at 19V, so this should give you a solid reference on how things should be in terms of components and how they change based off of system current differences.
Let me know if there are any more questions.
Best,
Krishan
1 Like