Hello dear.
I designed 5 pcb based on the Mp2235s, 4 of them work properly, but 1 of them, which is affected by ESD, does not produce 5V output. And its output is about 0 volts. I changed the regulator and inductor with new one, but it had no effect. The voltage on the SS pin is about 3.7V. schematic as following:
Hello,
Your schematics doesn’t seem to be the issue.
It is possible that the ESD has affected/damaged a different component on your board or the board itself.
I would recommend getting a fresh version of your board that does not have ESD damage.
Diagnosing the exact issue could take a long time and would be quite tedious.
I hope this helps.
Kind regards,
Eliza