MP2166 Synchronization Questions

Hi MPS Support,

We are evaluating the MP2166 for a dual-output design with 5 V nominal / 5.5 V maximum input, with outputs of 0.75 V at 1.1 A and 1.2 V at 0.4 A.

Could you please clarify:

  1. What is the maximum guaranteed minimum on-time over process and temperature?

  2. For the 5.5 V to 0.75 V rail, what is the maximum switching/synchronization frequency you would recommend?

  3. Can the SYNC input follow a spread-spectrum clock whose frequency is continuously modulated? If so, are there any important limits on the frequency range or modulation?

We are considering approximately 1–2 MHz operation.

Thanks,

Hi Dan,

Thank you for posting on the MPS Technical Forum.

  1. Min on-time is 55ns
  2. For 5V5 down to 0.75V, I would suggest not going above 2.4MHz. 1-2MHz is perfect.
  3. You will have to manually implement this on the SYNC pin. I would suggest choosing a switching frequency and going +/-50kHz for stability reasons.

Thanks,

Allison