I’m trying to calcluate the inductor value and it’s peak current needed. (also based updon the evaluation board) and I have difficulty why 3.3uH was chosen with such high current rating.
eg. Vin is between 2.5V and 5V ; Vout = 3.3V ; Load = 1 amp ; ripple at 20% ; I end up with values Lmin_buck = 5.61uH and Lmin_boost at 3.03uH
If I want to reduct the ripple to 10%, I end up with 11,22uH and 6,06 uH, so even for the evaluation board I never end up with 3,3uH as you have to choose the max value of these minimum L values.
Also the peak currents are much lower than the coils proposed in the BOM (they can handle 8amps or 10.1 amps and I get max currents of 4amps. So why this overkill in amp rating for the reference design?
Is my calculation wrong and if so why?
thanks